Hello Michael,The problem is that the STM32MCUwiki does not provide an example concerning the USB device. The examples only concern the USB power delivery which works well in my case with the STM32G0C1E-EV. Moreover, the problem is specific to some c...
Hi,I have the same issue with my STM32G0C1E-EV evaluation board.Furthermore, it also happens with my laptop (ubuntu) if I use a USB hub to connect the eval board.Using dmesg, I can see a difference, the evb is detected as a USB low speed device when ...
Hi, I am also using the STM32F072RB-Nucleo with the MB1257 version C expansion board with the analog front-end. I chose the DUAL_PORT_RTOS project among the different applications available in the archive. I have two different behaviors of the progra...