User Activity

HelloWe use the lps27hhw in our devices. When temperature is positive - all right. But when temperature is negative - the sensor sends the temperature less than it actually is (example -40* instead -20*). I put the appliance in the freezer, the tempe...
Hi everybody)I have a problem with exiting after shutdown mode. Entering codeif( (LL_PWR_IsActiveFlag_C1SB() == 0) || (LL_PWR_IsActiveFlag_C2SB() == 0) ) { /* Set the lowest low-power mode for CPU2: shutdown mode */ LL_C2_PWR_Set...
Hello,I have a board with stm32wb55. I can't enter to shutdown mode or can't to exit form shutdown.I want to exit from this mode via wakeup pin 1 PA0. I use this codeif( (LL_PWR_IsActiveFlag_C1SB() == 0) || (LL_PWR_IsActiveFlag_C2SB() == 0) ...
Good dayI can to open nothing *.pdf files on your site via Microsoft Edge (Microsoft Edge 44.17763.831.0; Microsoft EdgeHTML 18.17763). But via Google Chrome your site is working