I want to use LSM303AGR instead of LIS3MDL to detect a vehicle parking status. If i get the x-y-z component every second and calculate X=X_new - X_Previous, then new vehicle that comes near sensor is neglected after 1 second and i can't detect a veh...
Hello, i have a LSM303AGR sensor. According to what understood from this answer, i expect that my sensor x and y and z output (separately) be constant on various temperature (-40 °C to +85 °C), because of removing offset thermal drift. But that is no...