dchen.2000
Associate II
since
2019-12-04
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
1
Kudos received
View all badges
STMicroelectronics Community
About dchen.2000
Options
Report User
User Activity
Posts
Replies
document about "Teseo5 microcontroller with GNSS receiver capability for automotive and consumer applications"
2022-11-22
I want to get doc named “Teseo5 microcontroller with GNSS receiver capability for automotive and consumer applications�?, But I can not find in STA9100_SRTOS_Binary_Image_v5_10_19, where can i find it?Thank you very much!
Can ccmram be divided into data and BSS
2019-12-04
I want to divide ccmram into data and bss section,so how to do it?thank you!
Re: Can ccmram be divided into data and BSS
2019-12-05
#define CCMRAM __attribute__((section(".data_CCMRAM")))CCMRAM extern uint8_t ntripTxBuf[NTRIP_TX_BUFSIZE];lt iike this,it use RAM address not CCMRAM address. this is map: .data.udp_port 0x2000098e 0x2 .pio/build/OpenRTK/src/LWIP/l...
Re: Can ccmram be divided into data and BSS
2019-12-05
Thank you! I modify link file like this,but it does not work. so,why? .data_CCMRAM : ALIGN(4) { . = 0x20004000; test_ccm = 0x20004000; FILL(0xFF) *(.data.CCMRAM .data.CCMRAM.*) . = ALIGN(4) ; } > CCMRAM AT>FLASH .bss_C...
Kudos from
User
Count
Legacy member
1
View all