Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs Products
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
STM32 MPUs Products
STM32 MPUs Boards and hardware tools
STM32 MPUs Embedded software and solutions
STM32 MPUs Software development tools
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive and Transportation
Automotive MCUs
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
PGeuc.2036
Associate
since
2019-11-27
2023-06-14
User statistics
3
Posts
0
Solutions
0
Kudos given
1
Kudos received
View all badges
STMicroelectronics Community
About PGeuc.2036
Options
Report User
User Activity
Posts
Replies
I would like to knew why the GPIO-Pin PA11 is on high level while the Board boots. I configured the Pin Muxing with CubeMx and Loaded the Device tree for the Kernel in the boot directory and synced it. I configured the pin as a PWM pin.
2019-12-12
When I run my M4 Application every thing is working fine. But while the Board boots until i start the M4 remoteproc the pin is on high level. How can I set the pins reset(boot) configuration to low? I'am using the developer package.
I would like to know, if it is possible to debug the STM32MP157C-DK2 without the Serial Port (MPU Serial (/dev/ttyACM0)). I'm using the board in an mobile application and it would be very nice if I could debug the M4 like the A7 (only a GDBserver).
2019-12-05
Using the :STM32MP157C-DK2 STM32CubeIDE
Re: I would like to know, if it is possible to debug the STM32MP157C-DK2 without the Serial Port (MPU Serial (/dev/ttyACM0)). I'm using the board in an mobile application and it would be very nice if I could debug the M4 like the A7 (only a GDBserver).
2019-12-12
Thank you @Community member
Kudos from
User
Count
Legacy member
1
View all