Hello,sorry for the delay in responding.It seems from the command sequence that some steps might be missing for the M24SR to answer with no errors:As per NFC Forum specifications, it is necessary for the NDEF Tag Application Select command to be sent...
HelloThrough the SendInterrupt command it is not possible to pass any other parameters that would give information on a specific action to be taken by the micro.One example of what that could be done is to dedicate one location into the EEPROM for th...
Hi ,The error code 5 is not a value that the ST25TV02K PresentPassword RF command is returning. So we would need to know which subfunction of the rfalST25xVPollerPresentPassword is generating this error.Also could you please provide the values of A1S...
Hi Fabrice,by 'M24SR selected from the RF side', it is meant that the M24SR has been activated - meaning the phone has performed the technology detection, collision resolution, device activation). As you have indicated the new NDEF message can read f...
Hi FabriceIndeed RF_enable has to be set to 1 in order to allow M24SR to answer to phone's requests. Otherwise the M24SR will stay mute with respect to RF NFC commands.The bit in the system file is only writable from the I2C side so the MCU, and is n...