my data for this looks like the following without giving inputPA0 PA1 PA4 PA50 250 216 190I expect this PA0 PA1 PA4 PA50 0 0 0and when i start giving channel PA0 data wit...
I also found this thread as well, that i think would be useful but the Links given are dead and unhelpful. is there a template showing multiple channels of the ADC using a DMA?https://community.st.com/s/question/0D50X00009Xkgn8/stm32f072-adc-and-dma-...
Each pin is connected to a force sensor and about 3.3 volts. The force sensor is: Resistors Force Sensing Standard Round Format Connector HousingManufacturer #: FSR03CEAllied Stock #: 71202270and the specs and features of it are as follows:Series Fea...