Hi,On my target board I have implemented 14 pin JTAG interface as in STDC14 CN1 connector. Can I use ST-LINK/V2 debugger to flash and debug the controller..?The controller part is STM32F750V8. Please help with this.Thanks,Dhara
Hi,In the Linker Tab am I suppose to define any Scatter File (.SCT)..? As of now I am just keeping the default setting in the Keil Flash Config tool for Linker tab.Is there any link to download the AXIM Flash Algorithms for STMF7 controller..? Can yo...
Hi,I am not sure that controller is detected or not.. because I am not able to load my code but I am able to erase the in-chip Flash. I have written a code for GPIO toggling on my custom board with STM32F750V8 controllerI am trying to flash the contr...
Hi Uwe,Many thanks for replying..I have actually prepared that connector to interface my board (14pin) JTAG to ST Link V2 (20pin) debugger. But I am not able to flash the controller.Is this pin mapping correct.I referred the ST manual- UM1075 (Table ...