Hello,I found this interesting formula above in this thread, but I can#t figure out, what is the unit of n_max. If I use this formula for a typical stepper motor, I get a result of 0,000005787. Udc=24V, Ke=0,15V/Hz, Kstep=200.What is the unit of n_ma...
Posted on January 15, 2014 at 20:27>> not surprising, the STM32 external bus is designed for data storage, not for code execution << For our application we connected the ST32F407IG via FSMC to a 8-MBit SRAM (CY7C1051DV33). We have to execute the cod...