Hi everybody, I noticed that the accelerometric and gyroscopic signals are perturbed by an initial transient, like the one in the attached figure. What could be the issue?Thanks,Daniele
Hi everyone,Does the block data update mode block also the sensor's sampling? Or simply the sensor continues to acquire and the registers are just not updated until the next reading? It's very important to me because I use LSM9DS1 gyroscope and accel...
Hi Eleon,I'm now using the sensor in free running mode at 952 Hz (not anymore 119Hz) and the host is sampling at 100 Hz. If I understood correctly, BDU takes action only when the host reads the MSB (or LSB), therefore the host reads the nearest samp...