Dear Experts,I would like to start with the STM32H755 device, which shall have the interfaces,EthernetEthernet over SPIMay I have your inputs on identifying the eval board, Ethernet to SPI adapter card to start with?Thanks
Dear Experts,We have a design requirement with STM32H755 to work with Parallel Redundancy Protocol (PRP). Any relevant help or sources available.Thanks in advance.
Dear Experts,We have a design with STM32H755 having 3 Ethernet ports. Out of which 1 is over RMII controller the other two are over SPI interface.My queries are as follows,1. We want to run all 3 three Ethernets at the same time, How to handle this s...
Hi TDK,Thank you for your quick inputs.Actually I meant Ethernet over SPI interface, any related information/suggestions of PHY Dev's and it's driver support on STM32H755.-Thanks
Hi Pavel A,Glad to see your quick inputs.1. My doubt is about which platform supports this? Freertos or Embedded Linux or any?4. The requirement is to realise the Ethernet one with RMII and other 2 with SPI interface. So the managed switch is elim...
Hi Tesla DeLorean,Glad to see your quick inputs.1. Does this chipset supports Embedded Linux or FreeRTOS? Any reference or helpful links please?2. The requirement is to realise the Ethernet one with RMII and other 2 with SPI interface. So the manag...