User Activity

I am developing a motor controller with version 5.3.3 of the MC SDK.In the Basic tab of the Monitor, there is a Motor Power (W) indicator:It has an upper limit of 200 Watts.On the Registers tab, the same info can be seen:My question is, where does th...
Posted on December 17, 2013 at 04:24In version 1.2.0 of the CPAL I2C library, function CPAL_I2C_HAL_GPIODeInit(...) can fail when it calls the Standard Peripheral Library function GPIO_Init (...) due to  GPIO_InitStructure.GPIO_PuPd not being initia...