Today I've tried with a MDK Plus Trial license, because Hitex support did not know which MDK version is necessary for this processor.With MDK 5.29 I've got the same error as above (Internal Parameter error) and when using the newest MDK 5.35, I've go...
Hello Olivier,I checked both and I get the same error as above (internal parameter error).With STM32CubeIDE I can flash the same project. Any ideas?May this a problem, that the MDK essential version does not suffice for this processor (plus needed?)?...
Today I tried the to flash the "GPIO_EXTI" with MDK 5.29 and a MDK essential license in engieering mode to STM32MP157C-DK2.This time the error "no algorithm found" does not show with the same settings, but when trying to flash, an error dialog saysin...
Hello,I'm also having the same issue when trying to flash the M4 in engineering mode (B00T0 0, BOOT2 1) with KEIL µVision MDK-Lite V5.35.0.0"Load "GPIO_EXTI\\Debug\\GPIO_EXTI.axf" No Algorithm found for: 00000000H - 000003BBHNo Algorithm found for: 1...