User Activity

I have a design in which I am using an STM32L152VDT6 processor. The first prototype boards arrived, and one of the first things I noticed was that there was a resistance of 120 ohms between VCC and GND. I knew something had to be wrong at that point....
We have made good progress in migrating from an ST90R158 (ROMLESS) processor to an ST158E158 (EPROM). The issue we are now facing is that the code that is running in the ST90E will not run in the ST90T (will not even try to boot), which is our ultima...
We are currently trying to migrate a design from the ST90R to the ST90T (for supply reasons). We have been successful in reconfiguring the start vector in the ST90T to allow us to run from external ROM using the code developed for the ST90R. Unfortun...
Original post:https://community.st.com/s/question/0D50X00009Xkd3xSAB/its-possible-to-use-st90t158otp-as-rom-less-type-st90r158-help-me