Hey Clive and OZone, The Nucleo boards do not show up as a device at all. I have tried Win10 Desktop and Win7 Laptop. would i be able to use the ST-Link on the Disc board to program the Nucleo 144? Cheers
Thanks for the response Clive. I have tried multiple USB ports and having both connectors attach or just the ST-Link end. Windows will still not recognize that the board is connected. I can use the Discovery board with the same USB port and it works....