User Activity

Hello,I'm following this example: How to use the STM32 ADC's internal reference volt... - STMicroelectronics Community I'm using ADC4 rather than ADC1. I checked off Vrefint Channel and Vbat/4 Channel, and I let the IOC take care of the sequencing (i...
Hello,I'm looking for some troubleshooting advice. I saw a few tickets regarding this kind of problem and confirmed that __HAL_RCC_PWR_CLK_ENABLE() is called before setting the initial voltage scaling. This test code is completely auto-generated from...
Hello,I've successfully used the code below to enter shutdown on a U585CIUx. It wakes up on button press and I can tell it is coming up from reset because of timestamps (based on time since startup) and terminal output that only happens during startu...
Hello,I'm porting code that worked on STM32U585CI using SPI1 as full duplex master with GPDMA1 CH4(Rx)/CH5(Tx) to an STM32U585QII using SPI3, again as master with GPDMA1 CH4(Rx)/CH5(Tx). Only 1 SPI is used. I'm using CubeIDE 1.13.2 to autogenerate HA...
Hello,I've seen other posts provide links to examples for "USB host application based on the Audio OUT class". Are there any for audio in?Thanks
Kudos from