Posted on November 20, 2013 at 12:28 Hi Thiago, thanks for your response. I can now read / write the H3LIS331Dl :) But I have few questions! In the Datasheet from the H3LIS331DL the ''TyOff Typical zero-g level offset accuracy'' with +-1g is describ...
Posted on November 18, 2013 at 16:39Hi, I read that and I have also a few questions. I use the H3LIS331DL. I have no testboard, I use the chip direct with an µC (LPC1857), Are there any code examples ? I communicate over SPI. It works. I can read a...