User Activity

A daisy chain seems to be complicated because i can not configure the SPI chain in 4 wired at power up.Or, I would like to connect a specific CS on each LPS22HB and connect SCL / SDI / SDO together on the same SPI bus of the MCU. But I do not underst...
I'm using with cubemx the additional sotfware X-CUBE_MEMS1 with Terminal data logger and chose the mems LP22HB on a nucleo F401RE.When I do it in I2C it's working fine.No I configure the LP22HB in SPI with CS on GND. And connect for SPI. I configurat...