PShar.0.294
Associate II
since
2019-08-14
2023-06-14
User statistics
14
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About PShar.0.294
Options
Report User
User Activity
Posts
Replies
can timer interrupt wakeup STM32 from stop/Sleep mode ?
2019-08-23
Can i interface two different analog inputs to single pin(which is having two different ADC channels assigned ) of multi mode ADC in the STM32f205ZCCTTR. Can i scan those two with help of multimode ADC of STM32.?
2019-08-20
If can, please share the physical connection diagram (two Analog voltage sources to single pin micro controller ) and sample code for that.
In my application, I need to awake up with in 2 seconds regular intervals when it goes in stop mode. can you share sample code for RTC's calender and using its internal Alarm A for waking up?
2019-08-20
I am using STM32F030F4P6I am just looking for an example code where RTC gives a periodic alarm every 1 second (or any other time period)
hello I am using STM32F030F4 microcontroller, question is regarding low power mode. For that i want to wake from stop mode using RTC. As RTC programmable mode is not there in STM32F030F4, So what is the best way to awake from stop mode.
2019-08-14
Or any other way in STM32F030F4 microcontroller, to awake from low power mode. and I am using timer in my application.
Re: hello I am using STM32F030F4 microcontroller, question is regarding low power mode. For that i want to wake from stop mode using RTC. As RTC programmable mode is not there in STM32F030F4, So what is the best way to awake from stop mode.
2019-08-23
Dear SirDo you have a code snippet for periodic wakeup alarm for RTC at 1 sec?Thanks
Re: In my application, I need to awake up with in 2 seconds regular intervals when it goes in stop mode. can you share sample code for RTC's calender and using its internal Alarm A for waking up?
2019-08-23
I am using STM32F030F4P6. Possible for you to share code snippet for 1 second periodic wake in RTC.
Re: In my application, I need to awake up with in 2 seconds regular intervals when it goes in stop mode. can you share sample code for RTC's calender and using its internal Alarm A for waking up?
2019-08-23
I am using STM32F030F4P6. This does not have LPTIM
Re: In my application, I need to awake up with in 2 seconds regular intervals when it goes in stop mode. can you share sample code for RTC's calender and using its internal Alarm A for waking up?
2019-08-23
Dear Jack - can you please share a code snipped for RTC periodic wake up @ 1 Sec.I am using STM32F030F4P6
Re: Can i interface two different analog inputs to single pin(which is having two different ADC channels assigned ) of multi mode ADC in the STM32f205ZCCTTR. Can i scan those two with help of multimode ADC of STM32.?
2019-08-21
Thanks for response...
View more