cancel
Showing results for 
Search instead for 
Did you mean: 

Can i interface two different analog inputs to single pin(which is having two different ADC channels assigned ) of multi mode ADC in the STM32f205ZCCTTR. Can i scan those two with help of multimode ADC of STM32.?

PShar.0.294
Associate II

If can, please share the physical connection diagram (two Analog voltage sources to single pin micro controller ) and sample code for that.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ozone
Principal III

If I understand the question correct ...

Not at the same time. You would have to re-initialize the other setup each time you want to read the other channel.

If you short on pins, consider an external analog multiplexer. Similar to the 4067 / 74HC4067 CMOS device: https://en.wikipedia.org/wiki/List_of_4000-series_integrated_circuits

View solution in original post

2 REPLIES 2
Ozone
Principal III

If I understand the question correct ...

Not at the same time. You would have to re-initialize the other setup each time you want to read the other channel.

If you short on pins, consider an external analog multiplexer. Similar to the 4067 / 74HC4067 CMOS device: https://en.wikipedia.org/wiki/List_of_4000-series_integrated_circuits

PShar.0.294
Associate II

Thanks for response...