Hello. I am using the SPV1040 solar boost converter within the STEVAL-ISV012V1 development board. The datasheet states that the converter can work with an input voltage as low as 0.3 V. The solar cell I am using is able to provide 0.6 V (Voc) and 100...