Hi Martin, The SDRAM configuration was generated from the 429-DISC1 template. I dont see anywhere in this thread where the issue was fixed by reconfiguring SDRAM. I only see where CRamm.1 found that TouchGFX was hammering code. How do I fix the conf...
Or better yet, http://ge.tt/4W1PCo03 This is a clean project built with the cubeide 1.2.1 and touchgfx 4.13 for the 429-DISC1 dev boardOnly the call to the graphics processing loop has been added to the default task.
Martin KJELDSEN (ST Employee) - It might be easier if you could create a working "Hello world" project and stuff it here. Sounds like it'd only take you a few minutes. Would that be possible? using CubeIDE 1.2.1, TouchGFX 4.13.0 (see my comment on Cu...