User Activity

Hi all, my goal is to design a user can bootloader with for STM32F446 with IAR system.With the following process:A ready application code.design a bootloader code and output as .bin fileIn setting of application code, linker>input> choose bin filelin...
Posted on December 25, 2015 at 03:47Hi,I got a keil C project and try to add ADC peripheral into this peoject.I do believe this original project was made from STM Cube and did not enable ADC function in the begining.When I just add ADC init function...