I used STM32F103C8 series of chips, now I design four keys, the corresponding IOs is PC13,PC14,PC15 and PB11. The problem is that PC15 and PB11 cannot be used as input at the same time.As long as these two pins are not input at the same time, the res...