User Activity

Posted on December 14, 2015 at 12:44Hi all,I downloaded the library stm8s_dali_lib and tried to build the project using the ST Visual Develop v4.3.8I got error: ''Error creating proces for executable cxstm8''Has anyone had the same issue?Best regard...
Posted on April 08, 2015 at 17:04Hi, I am using the micro STM32L151 and I found that after programming the micro some of the micro have problems accesing FLASH and EEPROM.I can not program the micros again because it is not possible to read the FLAS...
Posted on February 27, 2015 at 11:43Hi,I am using the micro STM32L151. I am using it as an I2C slave and I am getting Overrun and AF errors.The SCL frequency is 100 KHz. When I used this micro as an I2C Slave at lower SCL frequencies it worked fine....
Posted on July 15, 2014 at 10:33Hi I am using thew micro STM32L151x8  and I am implementing the SPI driver. I want to use the SPI in master mode and only in transmiting mode. I am using for this purpose only 3 lines: NSS, MOSI and SCK. My first pro...
Posted on June 27, 2014 at 13:58Hi, I am using IAr Embedded for ARM. I programmed a ST32L151 micro but I configured the PA13(SWDAT) as a pull-down when it should be a pull-up and now I can not program again the micro. I tried to put a resistance to...