So I looked at the three firmware writes to see if they are corrupted and they appear to be shifted to the right by two bytes. The first two bytes for each of the the three writes are zeros and then it matches the firmware - for a while - too big to...
I am also having the exact same issue. I am getting random responses on two SATEL breakouts. After each hard reset, I get all zeros or random number in the four bytes that are read. It is peculiar that the poll for answer works as expected on the the...
What "send-2 bytes-function" ? The API only uses WrByte or WrMulti and that is all I set up in the platform files. I do not see where the API calls any other. Are you using the ULP provided by ST? Can you share any of the code?