Hello.We already have conference call to discuss this problem.It was identified that ADC clock was set to 170MHz, but ADC clock speed max is 60MHz. Due to this, ADC shows missing codes, etc.By reducing ADC clock, it should solve the problem.We also d...
Hello,As you are using output buffer, the output voltage is limited at 0.2V to VREF+-0.2V If output buffer is saturated, as output buffer is opamp structure, it's feedback is not correctly closed. then output voltage goes down it needs some time to ...
Posted on January 30, 2017 at 17:04Hello, Andrew.You are right, it looks like documentation is not inline.As far as I understood, the formula should be DACoutput = Vref x (DOR/4096)DAC is kind of R-2R implementation, Minimum code is corresponds to...
Posted on November 17, 2015 at 09:32Hello, Vinci. Sorry, I had difficulty of this web interface. I did TYPO in handler name, please use the original one. &hopamp_imotor Regards.