I'm using STM32F446RC controller CAN BUS 1. Trying to operate CAN BUS at 1mbps speed when using 100kbps bit rate it is working fine but not at 1Mbps bit rate. Is there any solution for this.
Hi @Community member The issue is solved. The problem is I was using USB CAN to send data to the CAN bus over controller seems like that was not working so I replaced it with controller to controller communication with the 60 MHz HSE clock with new ...
HI @Community member Thanks for your support.It is working now at 1Mbps baud rate. Actually I was sending data from USB CAN module to controller CAN, seems like it was not working so I tried controller to controller CAN communication it is working ...
Hi @Community member No, new parameters are not even working in loopback mode. I am using HSE Clock but even tried it with HSI but nothing works.I have checked that if I use 60 MHz clock for 100kbps baud rate below parameters (attaching below) with ...
Hello, @Community member I have tried these above mentioned parameters but still it does not work. It is working well at lower baud rates like 100kbps and 200kbps but not at 1mbps.