Yes, it is possible to power the NUCLEO-H743ZI2 board using the User USB instead of the ST-Link USB. You can connect the board to a power source through the User USB port. As for data transfer and debugging, you can use the ST-Link USB for both purpo...
1) Verify hardware connections and ensure everything is properly connected. 2) Review the code for correct configuration. 3) Test with different apps or examples to determine if the issue is with your code. 4) Ensure sufficient power, and up-to-date ...
After a power-loss reboot in STM32CubeIDE, there isn't a known list of specific issues. However, it's important to ensure proper initialization of variables, including floats, and review compatibility with CMSIS DSP library. Unexpected behavior in fl...