User Activity

TL;DR: is there an "ST approved" method to put have a custom machine's CubeMX project AND generated code under source control?I am trying to do something similar to OP's goal in this post, which didn't receive a full response, I think.I have also gon...
We need a DFU-capable bootloader for a custom board based on the STM32H750.We can't use the ROM bootloader due to 2 requirements:upload of the DFU image needs to happen over RS-485, with support for DE to an external transceiverwe need to flash the D...
Kudos given to