User Activity

In Cube, setting the Comparator to work with the DAC requires the DAC to be set as a GPIO however, I'd like to use the GPIO pins for other tasks, is this possible or does the DAC need to output on the GPIO for the comparator to work?
Posted on June 26, 2018 at 00:49Hi,I'm trying to enable the USB device peripheral for the STM32F042F4 in STM32CubeMX but it is greyed out and I don't seem to be able to enable it. I've checked the datasheet for this part and it seems to support USB ...
Posted on February 26, 2016 at 03:21Hi,I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperr...
Posted on February 26, 2016 at 03:20Hi,I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperr...
Posted on May 15, 2015 at 16:52Hi all,Throughout my time programming STM32 microcontrollers, I've used the standard peripheral libraries. Having recently designed my latest product around the STM32L051K8, I thought there would be a standard peripher...