User Activity

Hi Everyone.I use STM32F412G-DISCO to custom TFT 320x240 and set up the touchGFX the same.But when I generate the code it shows me the error "STM32F412G-DISCO.elf section `FramebufferSection' will not fit in region `RAMFB'I checked in the flash file....
Hi everyone.I have a board STM32F413 disco. How can I use TouchGFX to display on LCD on this board?I have found the template in TouchGFX but I didn't see it.Is there any way? that I can display LCD on the STM32F413 disco, or where I can find an examp...
Hi Everyone.I have tried test NFC use Nucleo-L152RE and X-Nucleo-NFC06A1.I use STM32duino X-NUCLEO-NFC06A1 example to test. It run normally with SPI interface.But when I change it to I2C interface, it can't run.Hardware modification: • so...
Hi everyone.I have STM32F769 Discovery-Board. I want to use this board control TFT 7inch using EK79007.How can I do it? Because i saw that EK79007 very different OTM8009 on STM32F769.Thanks.
Hi Everyone.I have plan to develop custom board based on kit STM32F769 Disco.TFTLCD I use in this project is 4-lane MIPI (https://focuslcds.com/content/E70RA-I-MW1530-C_Spec.pdf)But as we know STM32f769 Disco only have 2-lane MIPI.So I'm wondering wh...
Kudos from