Posted on October 14, 2013 at 15:04I have the STEVAL-MKI109V2 with the MKI135V1 accelerometer module. I've installed the Unico eval software v3.0.0.0. The COM port matches. There are no errors. I'm on Win7/64.There is no data.What am I missing?T...
Posted on November 18, 2013 at 23:00Hi Thiago,I was able to get some assistance from internal support through my sales rep.It seems that my version requires the latest Unico (v3.0.0.1) and a firmware upgrade.I hope to have a new demo kit by the end ...
Posted on October 22, 2013 at 19:21Hello Thiago,Thanks for responding. Whenever I change the setting away from Power Down Mode (Eg Normal 25Hz), nothing happens. If I switch to the Data screen, and then back to the Settings screen, it reverts to P...
Posted on October 21, 2013 at 15:20*bump*Anyone have a suggestion? I just need to show my boss that this device works, and then we can add a motion detect feature to our product.Thanks.