Posted on February 13, 2014 at 14:00I use stm32f4-discovery board. I am working with the ADCs, and for my prpose I need to set the ADC reference VREF+ at 3.2V. in the reference manual RM0090 it is said that stm32f4 LQFP100 has VREF+ VDDA pin. But th...
Posted on November 15, 2013 at 20:18Dear friends, I'll be using stm32f4 discovery with Matlab embedded coder. Now I'm not quite sure if this is the right place to ask for Matlab help,but my queries are solely related to the har...
Posted on September 27, 2013 at 09:17 Dear Sir, I'm using STM32F4-DISCOVERY. I've to run the STemWin on this board with keil RL-RTX. I've made all the necessary GUI and LCD configurations and have added GUI_X_RTX.c from the Segger folder in Keil uVi...
Posted on September 27, 2013 at 17:37I'm confident because I've run the demo without rtos. I've seen 2 rtos examples of emwin, one with freertos and the other with embos. And they are quite different from each other. So can't take them as reference ...