@Eleon BORLINI The overconsumption is due the VDD_IO pin being connected directly to the VCC.When I disconnect the VDD_IO pin from the VCC the consumption in Power-down mode goes to 5uA.
I changed the current consumption values in the sentences.The correct is:If CTRL1_XL has 0xA0 value, the consumption is 1,5mA -> It is goodif CTRL1_XL has 0x00 value, the consumption is 450uA -> it is not good.
@Eleon BORLINI Yes, you are correctly!I changed the current consumption values in the sentences.The correct is:If CTRL1_XL has 0xA0 value, the consumption is 1,5mA -> It is goodif CTRL1_XL has 0x00 value, the consumption is 450uA -> it is not good...
I'm using the development board STEVAL-MKI208V1.If CTRL1_XL has 0x00 value, the consumption is 1,5mA -> It is goodif CTRL1_XL has 0xA0 value, the consumption is 450uA -> it is not good.