Hello,The mentioned board utilizes usb otg communication through the USB connector. DM and DP pins are PA11 and PA12 which are directly connected from the mcu to the USB connector (no available GPIO pins). There is no usart or uart connected to the D...