User Activity

Hi,I'm working on a custom board where we integrated an STM32L010RB and I have verry weird behaviour :I need to use SPI1 peripheral and the clock signal is working as expected only if I enable optimization on the compiler settings.The MISO is OK. In ...
Hello,I'm working on a project using Zigbee as main communication network.In this project we develop two devices :One as server and coordinatorOne as client and routerWe based our hardware on STM32WB5MMG.I used the examples of Zigbee_OnOff_Client_Rou...