I am using the DMA2D to transfer colour data to an external SRAM using the FMC with an 8-bit parallel hardware setup. I can use the following line of code on the CM7 CPU to write to any in-range address (0x68000000 base) with any pointer type (uint8_...