Posted on July 05, 2018 at 14:24Hi all,the STEVAL-ISB038V1T cannot be Qi compliant since the Qi standard requires 5W min available power. The STEVAL-ISB038V1T power level is limited to 1W instead. By the way it uses the same protocol as Qi, so it m...
Posted on July 05, 2018 at 12:14Hi Janire,the material between TX and RX can be changed as long as it is not metallic. So any plastic, glass or wood is ok.It is recommended to keep a minimum spacer from the coil surface of 3mm. This is by default th...