User Activity

While I was looking for H7 DMA data,​I saw the article below that DMA is not working on the H7 device.https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices​Solution 1 from that article is shown below.​--------------------------...
Hi !​We are developing F746 MCU.​This issue occurred while developing the USB OTG HS USB Mass Storage function by referring to the example file in F7 CUBE.​It is normal to connect USB to MCU that operates as HOST and create new files with FATFS-based...
HI!​I'm currently working on a project using stm32F746-Disco board and Touchgfx.​As you know, The stm32F746-Disco board used 128 Mbit QSPI memory.​I'm running out of 128 Mbit SPI memory, so I'd like to use a higher capacity QSPI memory(256MBit).​​How...
Hi !​​I'm making a small project using Touchgfx and STM32F746.​I want to add video playback but I can't find any examples or projects to reference.​so, ​Can I get examples or projects of playing video using Touchgfx?(like MjpegReader in STM32H7Cube.....
I can't find "Configuring STM32F746g-DISCO" in TouchGFX Knowledge Base​There are only boards in the photo below​Please help..​