> So : WHAT is the problem then ? DMA not working correct ? Or not understanding, how it should work ?The problem is when using normal mode, the callback is called only once. second time I2S_Transmit_DMA return HAL_BUSY error. The reason why I want t...
I am not convinced with the answer. if somebody does not want to use circular mode then how he/she can do it?I am in the similar situation. Is there real solution to the problem?
@Fred @Jocelyn RICARD @pragnesh Sir,I am also implementing 2 image SBSFU on NUCLEO-H743ZI using STM32CubeExpansion_SBSFU_V2.6.1.I read all the SBSFU-related documents. I read the SBSFU integration guide also. Q1.would you like to confirm that the ...