Hello @ETann.1 ,what is your hardware setup? Which HelloWorld library are you using? Please, could you provide more information about your hardware and software setup?Best Regards,Carlo
Hello Sebastian,the Arduino library for X-NUCLEO-NFC06A1 was tested only with Nucleo boards in the Arduino environment. Anyway, the Arduino UNO does not have enough memory to run this library. I suggest to test it with a Nucleo board like for example...
Hello @PSław.1,Please, make sure to select ISM330DHCX Board Part as SPI, MOTION_SENSOR in the Board Support Custom in the X-CUBE-MEMS1 pack of CubeIDE and enable the correct pins for SPI and Chip Select. Make also sure that the Chip Select pin is ini...
Hi @Seenu ,it is really strange. I checked all the old versions of the MEMS package including also the v7.2.0 and I cannot find these APIs in the custom use case. As I know, these APIs at the moment are available only when you use the expansion boar...
Hello @Seenu ,we have checked in X-CUBE-MEMS1 v8.1.1 and we can say:CUSTOM_MOTION_SENSOR_DRDY_Enable_Interrupt() never existsCUSTOM_MOTION_SENSOR_DRDY_Set_Mode and other CUSTOM functions specific for particular sensor are only placeholders and needs...