Why do you need to write your personal DFU utility. For USB1, a DFU utility is inside the device bootloader click on button. Have a few switch early to your startup code to run DFU with a few marker Some magic in RAM or a few reset occasion.
This is just looking unbelievable I mean how's that possible if you are facing serial numbering issue you can have to contact with any expert of the field here.
Yes; also with contemporary isolators (the RF primarily based ones, now not vintage-fashion optoisolators) there's no cause for the low velocity when the ISOL board is established. It reduces the rate of STLINK V3 from 24MHz to 8MHz. I did checks and...
Yes; also with contemporary isolators (the RF primarily based ones, now not vintage-fashion optoisolators) there's no cause for the low velocity when the ISOL board is established. It reduces the rate of STLINK V3 from 24MHz to 8MHz. I did check and ...