Hi, Perhaps to look into a DK with MIPI allready supported and preferable same resoulution (or controller ILI9881C) for approx timing. But you need a better datasheet of the display controller.Then you need to find out if the panel need init codes an...
Hi Jalg.1Look into your <project>.touchgfx file : There should be some lines with the info."ApplicationTemplateVersion": "4.2.0","ApplicationTemplateDescription": "EDT Evaluation kit Application Template",
Thank you,My worries is that the application itself is running from the QSPI so I guess that you will need to jump away (execute from bootblock or RAM) while erasing and writing to the QSPI right ? Or do you rely on MCU being able to cache the code f...