Posted on May 17, 2011 at 13:28Quote:On 28-10-2009 at 18:20, Anonymous wrote: STM32F107 reference board uses the ''DP83848CVV'' (U$3.3 for 1k units), but there is the DP83848J (U$1,80 for 1k units). Someone has already used the DP83848J with the STM...
Posted on May 17, 2011 at 13:25Hello, I got a solution in the Keil forum; if someone is interested in, the link is http://www.keil.com/forum/docs/thread15723.asp . I checked the map file and the position was ok. Maybe the problem was that I programm...
Posted on May 17, 2011 at 13:25Hello, I'm trying to enable STM32 readout protection via Keil Ulink. I defined a ROM1 area starting from 0x1FFFF800 up to 0x1FFFF80F. I created a new c module containing two lines only: #include ''RTL.h'' const U32 opt...
Posted on May 17, 2011 at 13:22Hello, in the processor list, under download section, there's now a STM32W entry... inside it, there are the gerbers for a board named MB851 which use a STM32W108CBU processor... Can you give us some info about it, ple...
Posted on May 17, 2011 at 13:02Quote:On 11-02-2009 at 00:07, Anonymous wrote: If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :o Thank you! L