JPARK.42
Associate II
since
2021-06-07
2023-06-14
User statistics
5
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About JPARK.42
Options
Report User
User Activity
Posts
Replies
Hi, I am an assistant professor at Dept. of EE. I tough embedded system courses with Nucleo-64 F401 board. I want to use the newer evaluation board for the course which has a CAN controller. Is there a recommendation for it? Thanks
2021-06-07
Re: Hi, I am an assistant professor at Dept. of EE. I tough embedded system courses with Nucleo-64 F401 board. I want to use the newer evaluation board for the course which has a CAN controller. Is there a recommendation for it? Thanks
2021-06-08
Good information! Prototyping is important technique to the engineer. I will check those boards also. I appreciate your help.
Re: Hi, I am an assistant professor at Dept. of EE. I tough embedded system courses with Nucleo-64 F401 board. I want to use the newer evaluation board for the course which has a CAN controller. Is there a recommendation for it? Thanks
2021-06-08
Thanks for the information! This is a cheap and an interesting board! I will check it out.
Re: Hi, I am an assistant professor at Dept. of EE. I tough embedded system courses with Nucleo-64 F401 board. I want to use the newer evaluation board for the course which has a CAN controller. Is there a recommendation for it? Thanks
2021-06-08
Thanks for the quick response.One problem is that there is no built-in CAN controller in STM32F401xE (MCU of Nucleo-64 F401 board). That's why I am looking for the different evaluation board.
Re: Hi, I am an assistant professor at Dept. of EE. I tough embedded system courses with Nucleo-64 F401 board. I want to use the newer evaluation board for the course which has a CAN controller. Is there a recommendation for it? Thanks
2021-06-08
If possible, it's the best option. However, I can use the external transceiver.More important one is the budget which is less than 200$ / EA.