Posted on August 22, 2013 at 12:05I have chose the STM32F405RG and the st-link debugger.The program is used for STM32F407-DISCOVERY at first.It can work at the STM32F407-DICOVERY,but after I changed the device and other options.
Posted on August 23, 2013 at 07:39I was use the ''JTAG'' mode,and I'm sure that I have connected right in the light of the datasheet. But both BOOT0 and BOOT1 connect nothing.May it is wrong here?One more question,when I use I2C,the voltage is up to...