User Activity

I'm looking for a eval board/micro-controller with high-speed USB (with integrated PHY) and I2S interface to stream up to 12 audio channels (6-in/6-out) 16-bit samples at 44Khz. Are there any app-notes or recommendations on audio over high-speed USB...
Posted on May 17, 2018 at 21:31Hi, I am working with STM32Cube_FW_F7_V1.11.0 on a Nucleo_F746ZG.Seems like what I wanna do should be simple, but I'm not getting it...I need to measure the frequency of something, so I started with Projects/STM32F746Z...
Posted on March 14, 2018 at 14:03Hi, I'm not sure if this should be a discussion or a question, so I'm posting both...I'm hoping to hook up a Nucleo-F746ZG to an external codec eval board from Analog Devices.My current plan is to start with the AUDI...
Posted on August 26, 2013 at 22:45Hi, I'm trying to run the ''USB Device VCP example'' using the gcc (sourcery-lite) tools.  I can build it and it appears to be running (led is blinking and the message ''USB device library started'' comes out the UA...
Posted on August 16, 2013 at 17:15Hi, Being new to the list, I don't know if this will be of any interest, but i spent some time porting my boot monitor (http://www.umonfw.com) to the STM32F4 Discovery with the STM32F4DIS-BB expansion board.  I've b...