cancel
Showing results for 
Search instead for 
Did you mean: 

USB Audio on Nucleo-F746ZG?

Ed Sutter
Associate II
Posted on March 14, 2018 at 14:03

Hi, I'm not sure if this should be a discussion or a question, so I'm posting both...

I'm hoping to hook up a Nucleo-F746ZG to an external codec eval board from Analog Devices.

My current plan is to start with the AUDIO_Standalone application that comes with STM32Cube_FW_F7_V1.9.0 (for the STM32F769I_EVAL) and glue that into my Nucleo-F746ZG based platform.

Ignoring issues related to the different codec, is there any reason why I shouldn't be able to do this?

Thanks

#nucleo-f746 #stm32-audio-usb
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ed Sutter
Associate II
Posted on March 20, 2018 at 13:36

Well, apparently no interest here; but just to follow up on my own question for anyone reading this in the future...

I was able to do this on the Nucleo-F746ZG but simply starting with (and adjusting a bit) the '746 Discovery AUDIO_Standalone project.

Ed Sutter
Associate II
Posted on March 20, 2018 at 15:01

Well, perhaps I spoke too soon... 

The code as it stands now only runs as a audio output (usb speaker).  

There doesn't appear to be any support for usb-device audio input within stm32Cube.  

Can anyone confirm that this is true and if so, are there any examples elsewhere that demonstrate usb-device audio-input?