Hello Mr. Max,Thanks for the update.We are experimenting with the kit using the sample application- (SPC582Bxx_RLA_AEK_AUD_C1D9031 - Avas Compact - Test Application)We want to externally communicate with CAN channel for feeding Vehicle Speed and Moto...
Hello Mr. Max,Thanks for the update. Can you provide some information on the following points as well?The system is designed to work at 44kHz and this frequency cannot be increased.Q : We understand that the frequency cannot be increased, but can we ...
Hello ST Team,We need to know following information about this product:Current Consumption (no load, maximum)Operating Frequency RangeSound Pressure LevelMinimum frequency shift speedType of connector used Thanks & Regards,M.Siva